Below is a list of API functions output by the Code Generator for stand-by controller use.
Table 3.25
API Functions: [Stand-By Controller]
API Function Name
Function
R_STBC_Start_Stop_Mode
Start stand-by (STOP mode).
R_STBC_Prepare_Stop_Mode
Performs user-defined processing relating to the preparation to start stand-by (STOP mode).
R_STBC_Start_Deep_Stop_Mode
Start stand-by (DeepSTOP mode).
R_STBC_Prepare_Deep_Stop_Mode
Performs user-defined processing relating to the preparation to start stand-by (DeepSTOP mode).
R_STBC_Deep_Stop_Loop
Performs wait processing of stand-by (DeepSTOP mode).
R_STBC_Prepare_Stop_Mode_Set_Peripheral
Performs user-defined processing relating to the preparation (stop peripheral) to start stand-by (STOP mode).
R_STBC_Prepare_Stop_Mode_Set_Interrupt
Performs user-defined processing relating to the preparation (interrupt control register) to start stand-by (STOP mode).
R_STBC_Prepare_Stop_Mode_Set_Clock_Mask
Performs user-defined processing relating to the preparation (set the clock stop mask register) to start stand-by (STOP mode).
R_STBC_Prepare_Stop_Mode_Set_Clock_Source
Performs user-defined processing relating to the preparation (oscillate or stop each clock source) to start stand-by (STOP mode).
R_STBC_Prepare_Deep_Stop_Mode_Set_Peripheral
Performs user-defined processing relating to the preparation (stop peripheral) to start stand-by (DeepSTOP mode).
R_STBC_Prepare_Deep_Stop_Mode_Set_Interrupt
Performs user-defined processing relating to the preparation (interrupt control register) to start stand-by (DeepSTOP mode).