Everything
3.2.16 Timer Array Unit J

Below is a list of API functions output by the Code Generator for timer array unit J use.

Table 3.16

API Functions: [Timer array unit J]

API Function Name

Function

R_TAUJn_Create

Performs initialization necessary to control the timer array unit Jn.

R_TAUJn_Create_UserInit

Performs user-defined initialization relating to the timer array unit Jn.

r_taujn_channelm_interrupt

Performs processing in response to the timer interrupt.

R_TAUJn_Channelm_Start

Starts the count for channel m.

R_TAUJn_Channelm_Stop

Ends the count for channel m.

R_TAUJn_Channelm_Get_PulseWidth

Reads the input pulse width of the timer.