Below is a list of API functions output by the Code Generator for DTS use.
Table 3.6
API Functions: [DTS]
API Function Name
Function
R_DTS_Create
Performs initialization necessary to control the DTS functions.
R_DTS_Create_UserInit
Performs user-defined initialization relating to the DTS functions.
R_DTS_Suspend
Suspend DTS transfer.
R_DTS_Resume
Resume DTS transfer/
R_DTS_All_Stop
Stop all DTS transfer.
R_DTSx_y_Stop_Interrupt
Stop DTS transfer interrupt.
R_DTSm_Create
Performs initialization necessary to control the DTS channel m functions.
R_DTSm_Start
Enables the DTS channel m transfer.
R_DTSm_Stop
Disables the DTS channel m transfer.
R_DTSm_Set_SoftwareTrigger
Generates the DTS channel m transfer request.
R_DTSm_Suspend
Suspend DTS channel m transfer.
R_DTSm_Resume
Resume DTS channel m transfer.
R_DTSm_Create_UserInit
Performs user-defined initialization relating to the DTS channel m functions.
r_dtsx_y_transfer_match_interrupt
Performs processing in response to the DTS transfer match interrupt.
r_dtsx_y_transfer_completion_interrupt
Performs processing in response to the DTS transfer completion interrupt.