recipf.d


逆数(倍精度)を近似します。(Reciprocal of a Floating-point Value (Double))

[指定形式]

-

recipf.d reg1, reg2

[機能]

汎用レジスタreg1で指定されるレジスタ・ペアにある倍精度浮動小数点形式の内容の逆数を近似し,汎用レジスタreg2で指定されるレジスタ・ペアに格納します。演算結果はdivf命令を用いた結果と異なります。

[詳細説明]

-

アセンブラでは,機械語命令のrecipf.d命令が1つ生成されます。