recipf.s


逆数(単精度)を近似します。(Reciprocal of a Floating-point Value (Single))

[指定形式]

-

recipf.s reg1, reg2

[機能]

汎用レジスタreg1にある単精度浮動小数点形式の内容の逆数を近似し,汎用レジスタreg2に格納します。演算結果はdivf命令を用いた結果と異なります。

[詳細説明]

-

アセンブラでは,機械語命令のrecipf.s命令が1つ生成されます。