3.2.2 Clock generation circuit

Below is a list of API functions output by the Code Generator for clock generation circuit use.

Table 3.2

API Functions: [Clock Generation Circuit]

API Function Name

Function

R_CGC_Create

Performs initialization required to control the clock generation circuit.

R_CGC_Create_UserInit

Performs user-defined initialization relating to the clock generation circuit.

r_cgc_oscillation_stop_interrupt

Performs processing in response to the osillation stop detection interrupt.

r_cgc_oscillation_stop_nmi_interrupt

Performs processing in response to the oscillation stop detection NMI.

R_CGC_Set_ClockMode

Sets the clock source.