Renesas Electronics
Below is a list of API functions output by the Code Generator for port output enable 3 use.
Table 3.15
API Functions: [Port Output Enable 3]
API Function Name
Function
R_POE3_Create
Performs initialization necessary to control the port output enable 3.
R_POE3_Create_UserInit
Performs user-defined initialization relating to the port output enable 3.
r_poe3_oein_interrupt
Performs processing in response to the output enable interrupt n (OEIn).
R_POE3_Start
Places the MTU's complementary PWM output pins in the high-impedance state.
R_POE3_Stop
Releases the R_POE3_Stop MTU's complementary PWM output pins from the high-impedance state.
R_POE3_Set_HiZ_MTUn
Sets the high-impedance state for the MTUn pins.
R_POE3_Clear_HiZ_MTUn
Clear the high-impedance state for the MTUn pins.
R_POE3_Set_HiZ_GPTn
Sets the high-impedance state for the GPTn pins.
R_POE3_Clear_HiZ_GPTn
Clear the high-impedance state for the GPTn pins.