Renesas Electronics
Below is a list of API functions output by the Code Generator for watchdog timer use.
Table 3.23
API Functions: [Watchdog Timer]
API Function Name
Function
R_WDT_Create
Performs initialization necessary to control the watchdog timer.
R_WDT_Create_UserInit
Performs user-defined initialization relating to the watchdog timer.
r_wdt_nmi_interrupt
Performs processing in response to the non-maskable interrupt.
r_wdt_wuni_interrupt
Performs processing in response to the non-maskable/maskable interrupt.
R_WDT_Restart
Clears the watchdog timer counter and resumes counting.