3.2.37
LCD controller / driver (LCD)
Below is a list of API functions output by the Code Generator for LCD controller / driver use.
Table 3.37 | API Functions: [LCD controller / driver] |
|
|
R_LCD_Create
|
Performs initialization necessary to control the LCD controller / driver.
|
R_LCD_Create_UserInit
|
Performs user-defined initialization relating to the LCD controller / driver.
|
R_LCD_Start
|
Sets the LCD controller / driver to display on status.
|
R_LCD_Stop
|
Sets the LCD controller / driver to display off status.
|
R_LCD_Voltage_On
|
Enables operation of internal voltage boost circuit and capacitor split circuit.
|
R_LCD_Voltage_Off
|
Disables operation of internal voltage boost circuit and capacitor split circuit.
|