Renesas Electronics
Below is a list of API functions output by the Code Generator for D/A converter use.
Table 3.31
API Functions: [D/A Converter]
API Function Name
Function
R_DA_Create
Performs initialization necessary to control the D/A converter.
R_DA_Create_UserInit
Performs user-defined initialization relating to the D/A converter.
R_DAm_Start
Starts D/A conversion.
R_DAm_Stop
Ends D/A conversion.
R_DAm_Set_ConversionValue
Sets the data for D/A conversion.