Below is a list of API functions output by the Code Generator for Comparator C use.
Table 3.36 API Functions: [Comparator C]
API Function Name |
Function |
Performs initialization necessary to control the Comparator C. | |
Performs user-defined initialization relating to the Comparator C. | |
Performs processing in response to the comparator C interrupt. | |
Starts comparison for analog input voltage. | |
Ends comparison for analog input voltage. |