General PWM timer (GPT)

Below is a list of API functions output by the Code Generator for general PWM timer use.

Table 3.16 API Functions: [General PWM timer]

API Function Name

Function

R_GPT_Create

Performs initialization necessary to control the general PWM timer.

R_GPTn_Start

Starts counting by a 16-bit timer.

R_GPTn_Stop

Ends counting by a 16-bit timer.

R_GPTn_HardwareStart

Allows GPT interrupts.

R_GPTn_HardwareStop

Prohibits GPT interrupts.

R_GPT_Create_UserInit

Performs user-defined initialization relating to the general PWM timer.

r_gpt_gtcimn_interrupt

Performs processing in response to the input capture/compare match interrupt.

r_gpt_gtcivn_interrupt

Performs processing in response to the overflow interrupt.

r_gpt_gtciun_interrupt

Performs processing in response to the underflow interrupt.

r_gpt_gdten_interrupt

Performs processing in response to the dead time error interrupt.

r_gpt_etgip_interrupt

Performs processing in response to the external trigger rising interrupt.

r_gpt_etgin_interrupt

Performs processing in response to the external trigger falling interrupt.