Low power timer (LPT)

Below is a list of API functions output by the Code Generator for low power timer use.

Table 3.35 API Functions: [Low power timer]

API Function Name

Function

R_LPT_Create

Performs initialization necessary to control the low power timer.

R_LPT_Create_UserInit

Performs user-defined initialization relating to the low power timer.

R_LPT_Start

Starts counting by a low power timer.

R_LPT_Stop

Ends counting by a low power timer.