Serial peripheral interface (RSPI)

Below is a list of API functions output by the Code Generator for serial peripheral interface use.

Table 3.28 API Functions: [Serial Peripheral Interface]

API Function Name

Function

R_RSPIn_Create

Performs initialization necessary to control the serial peripheral interface.

R_RSPIn_Create_UserInit

Performs user-defined initialization relating to the serial peripheral interface.

r_rspin_receive_interrupt

Performs processing in response to the receive buffer full interrupts.

r_rspin_transmit_interrupt

Performs processing in response to the transmit buffer error interrupts.

r_rspin_error_interrupt

Performs processing in response to the RSPI error interrupts.

r_rspin_idle_interrupt

Performs processing in response to the RSPI idle interrupts.

R_RSPIn_Start

Starts RSPI communication.

R_RSPIn_Stop

Ends RSPI communication.

R_RSPIn_Send

Starts RSPI transmission.

R_RSPIn_Send_Receive

Starts RSPI transmission/reception.

r_rspin_callback_receiveend

Performs processing in response to the receive buffer full interrupts.

r_rspin_callback_error

Performs processing in response to the RSPI error interrupts.

r_rspin_callback_transmitend

Performs processing in response to the RSPI idle interrupts.