Below is a list of API functions output by the Code Generator for watchdog timer use.
Table 3.23 API Functions: [Watchdog Timer]
API Function Name |
Function |
Performs initialization necessary to control the watchdog timer. | |
Clears the watchdog timer counter and resumes counting. | |
Performs user-defined initialization relating to the watchdog timer. | |
Performs processing in response to the non-maskable/maskable interrupt. | |
Performs processing in response to the non-maskable interrupt. |