Low power consumption

Below is a list of API functions output by the Code Generator for low power consumption use.

Table 3.5 API Functions: [Low Power Consumption]

API Function Name

Function

R_LPC_Create

Performs initialization required to control the low power consumption.

R_LPC_Create_UserInit

Performs user-defined initialization relating to the low power consumption.

R_LPC_AllModuleClockStop

Stops the clock for all modules.

R_LPC_ChangeSleepModeReturnClock

Sets the clock source that is selected following release from sleep mode.

R_LPC_Sleep

Transits the low power consumption mode of the MCU to the sleep mode.

R_LPC_DeepSleep

Transits the low power consumption mode of the MCU to the deep sleep mode.

R_LPC_DeepSoftwareStandby

Transits the low power consumption mode of the MCU to the deep software standby mode.

R_LPC_SoftwareStandby

Transits the low power consumption mode of the MCU to the software standby mode.

R_LPC_ChangeOperatingPowerControl

Changes the operating power control mode of the MCU.