Data operation circuit (DOC)

Below is a list of API functions output by the Code Generator for data operation circuit.

Table 3.34 API Functions: [Data Operation Circuit]

API Function Name

Function

R_DOC_Create

Performs initialization necessary to control the data operation circuit.

R_DOC_Create_UserInit

Performs user-defined initialization relating to the data operation circuit.

r_doc_dopcf_interrupt

Performs processing in response to the data operation circuit interrupt.

R_DOC_SetMode

Sets the operating mode and the initial value of the reference value for use by the data operation circuit.

R_DOC_WriteData

Sets the input value (value for comparison with, addition to, or subtraction from the reference value) for use by the data operation circuit.

R_DOC_GetResult

Gets the result of operation.

R_DOC_ClearFlag

Clears the data operation circuit flag.