3.2.49 Operational amplifier and Analog switch

Below is a list of API functions output by the Code Generator for Operational Amplifier and Analog switch use.

Table 3.49

API Functions: [Operational amplifier and Analog switch]

API Function Name

Function

R_AMPANSW_Create

Performs initialization necessary to control the Operational amplifier and Analog switch.

R_AMPANSW_Create_UserInit

Performs user-defined initialization relating to the Operational amplifier and Analog switch.

R_OPAMPm_Set_ReferenceCurcuitOn

Enables operational amplifier reference current circuit.

R_OPAMPm_Set_ReferenceCircuitOff

Disables operational amplifier reference current circuit.

R_OPAMPm_Start

Starts operational amplifier of unit m.

R_OPAMPm_Stop

Stops operational amplifier of unit m.

R_ANSW_ChargePumpm_On

Enables analog switch of unit m.

R_ANSW_ChargePumpm_Off

Disables analog switch of unit m.