3.2.43 SPI interface

Below is a list of API functions output by the Code Generator for SPI interface use.

Table 3.43

API Functions: [SPI Interface]

API Function Name

Function

R_SAIC_Create

Performs initialization necessary to control the SPI interface.

R_SAIC_Create_UserInit

Performs user-defined initialization relating to the SPI interface.

R_SAIC_Write

Starts SPI data transmission.

R_SAIC_Read

Starts SPI data reception.