3.2.39 Key interrupt function

Below is a list of API functions output by the Code Generator for key interrupt function use.

Table 3.39

API Functions: [Key Interrupt Function]

API Function Name

Function

R_KEY_Create

Performs initialization necessary to control the key interrupt function.

R_KEY_Create_UserInit

Performs user-defined initialization relating to the key interrupt function.

r_key_interrupt

Performs processing in response to the key interrupt INTKR.

R_KEY_Start

Enables the acceptance of the key interrupt INTKR.

R_KEY_Stop

Disables the acceptance of the key interrupt INTKR.