3.2.14 Subsystem clock frequency measurement circuit

Below is a list of API functions output by the Code Generator for subsystem clock frequency measurement circuit use.

Table 3.14

API Functions: [Subsystem Clock Frequency Measurement Circuit]

API Function Name

Function

R_FMC_Create

Performs initialization necessary to control the subsystem clock frequency measurement circuit.

R_FMC_Create_UserInit

Performs user-defined initialization relating to the subsystem clock frequency measurement circuit.

r_fmc_interrupt

Performs processing in response to the end of frequency measurement interrupt INTFM.

R_FMC_Start

Starts measurement of the frequency that uses the subsystem clock frequency measurement circuit.

R_FMC_Stop

Ends measurement of the frequency that uses the subsystem clock frequency measurement circuit.

R_FMC_Set_PowerOff

Halts the clock supplied to the subsystem clock frequency measurement circuit.