3.2.22 Configurable amplifier

Below is a list of API functions output by the Code Generator for configurable amplifier use.

Table 3.22

API Functions: [Configurable amplifier]

API Function Name

Function

R_CAMP_Create

Performs initialization necessary to control the configurable amplifier.

R_CAMP_Create_UserInit

Performs user-defined initialization relating to the configurable

amplifier.

R_CAMPn_Start

Turns on the power of the configurable amplifier(AMPn).

R_CAMPn_Stop

Turns off the power of the configurable amplifier(AMPn).

R_CAMP_Set_PowerOff

Halts the clock supplied to the configurable amplifier.