3.2.4 High-speed on-chip Oscillator clock Frequency Correction function

Below is a list of API functions output by the Code Generator for the High-speed on-chip Oscillator clock Frequency Correction function use.

Table 3.4

API Functions: [High-speed on-chip Oscillator clock Frequency Correction function]

/

API Function Name

Function

R_HOFC_Create

Performs initialization necessary to control the High-speed on-chip Oscillator clock Frequency Correction function.

R_HOFC_Create_UserInit

Performs user-defined initialization relating to the High-speed on-chip Oscillator clock Frequency Correction function.

r_hofc_interrupt

Performs processing in response to the timer interrupt.

R_HOFC_Start

Starts the count for the High-speed on-chip Oscillator clock Frequency Correction function.

R_HOFC_Stop

Ends the count for the High-speed on-chip Oscillator clock Frequency Correction function.