3.2.11 16-bit timer KC0

Below is a list of API functions output by the Code Generator for 16-bit timer KC0 use.

Table 3.11

API Functions: [16-bit Timer KC0]

API Function Name

Function

R_TMR_KC0_Create

Performs initialization necessary to control the 16-bit timer KC0.

R_TMR_KC0_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer KC0.

r_tmr_kc0_interrupt

Performs processing in response to the timer interrupt.

R_TMR_KC0_Start

Starts the count for 16-bit timer KC0.

R_TMR_KC0_Stop

Ends the count for 16-bit timer KC0.

R_TMR_KC0_Set_PowerOff

Halts the clock supplied to the 16-bit timer KC0.