3.2.26 Programmable gain amplifier

Below is a list of API functions output by the Code Generator for programmable gain amplifier use.

Table 3.26

API Functions: [Programmable Gain Amplifier]

API Function Name

Function

R_PGA_Create

Performs initialization necessary to control the programmable gain amplifier.

R_PGA_Create_UserInit

Performs user-defined initialization relating to the programmable gain amplifier.

R_PGA_Start

Starts the operation of programmable gain amplifier.

R_PGA_Stop

Ends the operation of programmable gain amplifier.

R_PGA_Reset

Reset the programmable gain amplifier.

R_PGA_Set_PowerOff

Halts the clock supplied to the programmable gain amplifier.