3.2.37 Event link controller

Below is a list of API functions output by the Code Generator for event link controller (ELC) use.

Table 3.37

API Functions: [Event Link Controller]

API Function Name

Function

R_ELC_Create

Performs initialization necessary to control the event link controller (ELC).

R_ELC_Create_UserInit

Performs user-defined initialization relating to the event link controller (ELC).

R_ELC_Stop

Disables operation of the event link controller (ELC).