3.2.41 Battery backup function

Below is a list of API functions output by the Code Generator for battery backup function use.

Table 3.41

API Functions: [Battery Backup Function]

API Function Name

Function

R_BUP_Create

Performs initialization necessary to control the battery backup function.

R_BUP_Create_UserInit

Performs user-defined initialization relating to the battery backup function.

r_bup_interrupt

Performs processing in response to the power switching detection interrupt INTVBAT.

R_BUP_Start

Enables operation of battery backup function.

R_BUP_Stop

Disables operation of battery backup function.