3.2.50 Voltage reference

Below is a list of API functions output by the Code Generator for voltage Reference use.

Table 3.50

API Functions: [Voltage Reference]

API Function Name

Function

R_VR_Create

Performs initialization necessary to control the Voltage reference.

R_VR_Create_UserInit

Performs user-defined initialization relating to the Voltage reference.

R_VR_Start

Enables operation of Voltage reference.

R_VR_Stop

Disables operation of Voltage reference.