Below is a list of API functions output by the Code Generator for 12-bit A/D converter use.
Table 3.49 API Functions: [12-bit A/D Converter]
API Function Name |
Function |
Performs initialization necessary to control the 12-bit A/D converter. | |
Performs user-defined initialization relating to the 12-bit A/D converter. | |
Performs processing in response to the A/D conversion end interrupt INTAD. | |
Starts A/D conversion. | |
Ends A/D conversion. | |
Reads the results of A/D conversion (12 bits). | |
Configures the analog voltage input pin for A/D conversion. | |
Enables 12-bit A/D converter temperature sensor output circuit. | |
Disables12-bit A/D converter temperature sensor output circuit. | |
Enables 12-bit A/D converter reference voltage circuit. | |
Disables12-bit A/D converter reference voltage circuit. | |
Halts the clock supplied to the 12-bit A/D converter. |