Below is a list of API functions output by the Code Generator for key interrupt function use.
Table 3.41 API Functions: [Key Interrupt Function]
API Function Name |
Function |
Performs initialization necessary to control the key interrupt function. | |
Performs user-defined initialization relating to the key interrupt function. | |
Performs processing in response to the key interrupt INTKR. | |
Enables the acceptance of the key interrupt INTKR. | |
Disables the acceptance of the key interrupt INTKR. |