Below is a list of API functions output by the Code Generator for Operational Amplifier and Analog switch use.
Table 3.51 API Functions: [Operational amplifier and Analog switch]
| API Function Name | Function | 
| Performs initialization necessary to control the Operational amplifier and Analog switch. | |
| Performs user-defined initialization relating to the Operational amplifier and Analog switch. | |
| Enables operational amplifier reference current circuit. | |
| Disables operational amplifier reference current circuit. | |
| Starts operational amplifier of unit m. | |
| Stops operational amplifier of unit m. | |
| Enables analog switch of unit m. | |
| Disables analog switch of unit m. |