Everything
 

Current Consumption Measurement Search dialog box [E2]


This dialog box is used to specify and search the detailed conditions in the Measuring Current Consumption panel [E2].

Caution

Measuring current consumption is only available for the RX100 and RX200 Series.

Figure A.53

Current Consumption Measurement Search Dialog Box

 

This section describes the following.

[How to open]

-

On the Measuring Current Consumption panel [E2], click the button on the toolbar.

[Description of each area]

(1)

[Searching option] area

Specify the search conditions.

(a)

[Condition]

Select the type of the search conditions from the following drop-down list.

Over threshold

Detect the moment when the current being measured becomes or exceeds a specified value.

Under Threshold

Detect the moment when the current being measured becomes or falls below a specified value.

In range

Detect the moment when the current being measured enters a specified range of values.

Out of Range

Detect the moment when the current being measured leaves a specified range of values.

Monitor point

Detect the specified monitoring point.

(b)

[Current value]

Specify the specific value or range of values for current to serve as the search condition in microamperes.

Specify one value for current when "Over threshold" or "Under Threshold" is selected for [Condition], and two values for current when "In range" or "Out of Range" is selected for [Condition].

Caution

For a range of current values, the value entered in the left field for entry must be lower than that in the right field.

(c)

[Specify detecting width]

When "Over threshold", "Under Threshold", or "In range" is selected for [Condition], specify whether the data is only searched when the change in the value for current continues for a specific period or at the instant the required change in the value is detected.

To search the data, select the check box and specify the condition for the interval and the interval.

<1>

Condition for the interval

Select the condition for the interval from the following drop-down list.

Over threshold

Detect the data when the condition specified for [Condition] continues to be satisfied for at least the specified interval.

In range

Detect the data only when the condition specified for [Condition] continues to be satisfied within the specified interval.

<2>

Interval

Specify a multiple of the sampling time selected for [Sampling time] in the Current Consumption Measurement Condition Setting dialog box [E2].

The actual interval is the specified multiple of the sampling time.

(d)

[Monitor point]

When "Monitor point" is selected for [Condition], select "All" or the current monitoring point as the target monitoring point.

[Function buttons]

Button

Function

Find First

Searches the whole of the measured data from its start for points that satisfy the conditions specified in this dialog box.

Find Previous

Searches forward in time from the position of the cursor in the graph display area in the Measuring Current Consumption panel [E2] for the points that satisfy the conditions specified in this dialog box.

Find Next

Searches backward in time from the position of the cursor in the graph display area in the Measuring Current Consumption panel [E2] for the points that satisfy the conditions specified in this dialog box.

Find Last

Searches the whole of the measured data from its end for points that satisfy the conditions specified in this dialog box.

Close

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.