Everything

debugger.SoftwareTraceLPD.Get


This function refers to the software trace (LPD output) data for the specified number of frames.

This function also outputs the acquired software trace (LPD output) data to a file. [RH850][E2]

[Specification format]

debugger.SoftwareTraceLPD.Get(frameCount, fileName = "", append = False)

[Argument(s)]

Argument

Description

frameCount

Specify the number of frames for which software trace (LPD output) data is acquired.

fileName

Specify the full path of the file name to which data will be output (default: not specified).

append

Specify whether to append software trace (LPD output) data to the file.

True: Append software trace data to the file.

False: Do not append software trace data to the file (default).

[Return value]

Software trace data (LPD output) (see the SoftwareTraceInfo class for detail)

If there is no data, None is set.

[Detailed description]

-

The software trace (LPD output) data is shown by the following format.

 

When the microcontroller is single core:

-

DBCP

number-of-frames timestamp PC DBCP

-

DBTAG (with PC)

number-of-frames timestamp PC category data DBTAG

-

DBTAG (without PC)

number-of-frames timestamp category data DBTAG

-

DBPUSH (with PC)

number-of-frames timestamp PC register-ID register-data DBPUSH

-

DBPUSH (without PC)

number-of-frames timestamp register-ID register-data DBPUSH

 

When the microcontroller is multi-core:

-

DBCP

number-of-frames PE-number timestamp PC DBCP

-

DBTAG (with PC)

number-of-frames PE-number timestamp PC category data DBTAG

-

DBTAG (without PC)

number-of-frames PE-number timestamp category data DBTAG

-

DBPUSH (with PC)

number-of-frames PE-number timestamp PC register-ID register-data DBPUSH

-

DBPUSH (without PC)

number-of-frames PE-number timestamp register-ID register-data DBPUSH

[Example of use]

>>>trace = debugger.SoftwareTraceLPD.Get(100)
 99  00h00min00s003ms702us000ns 0x00001028 0x03 0x20 DBTAG
 99  00h00min00s003ms702us000ns 0x00001030 0x03 0x0020 DBPUSH
100  00h00min00s003ms702us000ns 0x00001032 DBCP
>>>