Everything

debugger.Timer.Clear


This function clears the result measured by a conditional timer.

[Specification format]

debugger.Timer.Clear()

[Argument(s)]

None

[Return value]

If the result measured by a conditional timer was cleared successfully: True

If there was an error when clearing the result measured by a conditional timer: False

[Detailed description]

-

This function clears the result measured by a conditional timer.

[Example of use]

>>>debugger.Timer.Get()
1 Total: 2000 ns, Pass Count: 4 , Average: 500 ns, Max: 800 ns, Min: 300 ns
>>>debugger.Timer.Clear()
True
>>>debugger.Timer.Get()
1 Total: 0 ns, Pass Count: 0 , Average: 0 ns, Max: 0 ns, Min: 0 ns
>>>