Everything

debugger.Breakpoint.Disable


This function disables a break point setting.

[Specification format]

debugger.Breakpoint.Disable(breakNumber = "")

[Argument(s)]

Argument

Description

breakNumber

Specify the break event number to disable.

[Return value]

If a break point setting was disabled successfully: True

If there was an error when disabling a break point setting: False

[Detailed description]

-

This function disables the break event specified by breakNumber.

-

If breakNumber is not specified, then breaks of all break event numbers will be disabled.

[Example of use]

>>>debugger.Breakpoint.Enable(1)
True
>>>debugger.Breakpoint.Disable(1)
True
>>>debugger.Breakpoint.Delete(1)
True
>>>