Everything

debugger.GetCpuStatus


This function displays the current CPU status.

[Specification format]

debugger.GetCpuStatus()

[Argument(s)]

None

[Return value]

Current CPU status (string)

CPU Status

Description

Hold

In bus hold

HoldStopIdle

Bus hold/Software STOP/Hardware STOP/IDLE mode

PowOff

Power not supplied to the target

InitialStop

Initial stop

Reset

In reset state

Standby

GTM: Clock is not supplied

Other than GTM: In standby mode

Stop

In STOP mode

StopIdle

Software STOP/Hardware STOP/IDLE mode

Wait

In wait state

Halt

In HALT mode

Sleep

In sleep state

DeepStop

In Deep Stop mode

CyclicRun

In Cyclic Run mode

CyclicStop

In Cyclic Stop mode

CyclicDisable

This is the state of the core other than the main core when the main core is in the Cyclic Run or Cyclic Stop mode.

Disable

MCS of GTM is not running.

None

N/A

[Detailed description]

-

This function displays the current CPU status.

[Example of use]

>>>debugger.GetCpuStatus()
Stop
>>>