Everything

debugger.Timer.Delete


This function deletes a conditional timer.

[Specification format]

debugger.Timer.Delete(timerNumber = "")

[Argument(s)]

Argument

Description

timerNumber

Specify the timer event number to delete.

[Return value]

If a timer was deleted successfully: True

If there was an error when deleting a timer: False

[Detailed description]

-

This function deletes the timer of the timer event number specified by timerNumber.

-

If timerNumber is not specified, then timers of all timer event numbers will be deleted.

[Example of use]

>>>debugger.Timer.Delete(1)
True
>>>