Everything

debugger.Connect


This function connects to the debug tool.

[Specification format]

debugger.Connect()

[Argument(s)]

None

[Return value]

If the debug tool was connected successfully: True

If there was an error when connecting to the debug tool: False

[Detailed description]

-

This function connects to the debug tool.

[Example of use]

>>>debugger.Connect()
True
>>>