debugger.Interrupt.RequestFENMI
|
This function sends an NMI request to the interrupt controller. [RH850 Simulator (G4MH)]
[Specification format]
debugger.Interrupt.RequestFENMI()
|
[Argument(s)]
None
[Return value]
If the interrupt request was successful : True
If the interrupt request failed : False
[Detailed description]
- | This function sends an NMI request to the interrupt controller. |
- | Generation of the interrupt depends on the settings and state of the interrupt controller. |
[Example of use]
>>>debugger.Interrupt.RequestFENMI()
True
>>>
|