Everything

debugger.Timer.Set


This function sets a conditional timer.

[Specification format]

debugger.Timer.Set(TimerCondition)

[Argument(s)]

Argument

Description

TimerCondition

Specify a condition of a conditional timer.

See the TimerCondition class for creating a conditional timer.

[Return value]

Set timer event number (numerical value)

[Detailed description]

-

This function sets a conditional timer according to the contents specified with TimerCondition.

-

The specified conditional timer is registered with the following name.
number is a four-digit decimal.

Python Timer number

[Example of use]

>>>tc = TimerCondition()
>>>tc.StartAddress = "main"
>>>tc.EndAddress = "chData"
>>>tc.EndData = 0x20
>>>tc.EndTimerType = TimerType.Write
>>>ts_number = debugger.Timer.Set(tc)
1
>>>print ts_number
1