Everything

debugger.IsRunning


This function checks the execution status of the user program.

[Specification format]

debugger.IsRunning()

[Argument(s)]

None

[Return value]

If the user program is running: True

If the user program is not running: False

[Detailed description]

-

This function checks the execution status of the user program.

[Example of use]

>>>if debugger.IsRunning() == True :
...  print "OK"
...
True
OK
>>>