Everything

debugger.SoftwareTraceLPD.Set


This function sets a software trace (LPD output). [RH850][E2]

[Specification format]

debugger.SoftwareTraceLPD.Set(DBCP, DBTAG, DBPUSH, PC = True, PE)

[Argument(s)]

Argument

Description

DBCP

Specify whether to acquire the results of DBCP.

True: Acquire the results of DBCP.

False: Do not acquire the results of DBCP.

DBTAG

Specify whether to acquire the results of DBTAG.

True: Acquire the results of DBTAG.

False: Do not acquire the results of DBTAG.

DBPUSH

Specify whether to acquire the results of DBPUSH.

True: Acquire the results of DBPUSH.

False: Do not acquire the results of DBPUSH.

PC

Specify whether to include information of the PC address in the results of DBTAG and DBPUSH.

True: Include information of the PC address (default).

False: Do not include information of the PC address.

PE

If the device is multi-core, specify the number of the core from which you wish to acquire trace information.

Specification of this argument is ignored if the device in use only has one core.

[Return value]

If a software trace (LPD output) was set successfully: True

If there was an error when setting a software trace (LPD output): False

[Detailed description]

-

This function sets a software trace (LPD output).

[Example of use]

>>>debugger.SoftwareTraceLPD.Set(True,True,False,False,1)
True
>>>