Everything

debugger.Breakpoint.Information


This function displays break point information.

[Specification format]

debugger.Breakpoint.Information()

[Argument(s)]

None

[Return value]

List of break point information (see the BreakpointInfo property for detail)

[Detailed description]

-

This function displays the break point settings in the following format.

break-event-number break-name state address-location

[Example of use]

>>>debugger.Breakpoint.Information()
   1 PythonBreak0001 Enable  0x000002dc
   2 Break0001 Enable  test1.c#_sub1
   3 PythonBreak0002 Enable  0x000002ec
   4 Break0002 Enable  test1.c#_sub1+10
>>>