Everything

debugger.DebugTool.SaveState


This function saves the state of the debug tool to a file.

[Specification format]

debugger.DebugTool.SaveState(fileName)

[Argument(s)]

Argument

Description

fileName

Specify the full path of the file to save the state of the debug tool.

[Return value]

If the file was saved successfully: True

If there was an error when saving the file: False

[Detailed description]

-

This function saves readable/writable memory and register values to a file as the state of the debug tool.

[Example of use]

>>>debugger.DebugTool.SaveState("C:/test/debugtoolstate.log")
True
>>>