Everything

debugger.Timer.Get


This function references the result measured by a conditional timer.

[Specification format]

debugger.Timer.Get()

[Argument(s)]

None

[Return value]

List of conditional timer information (see the TimerInfo class for detail)

[Detailed description]

-

The result measured by a conditional timer is shown by the following format.

timer-event-number Total: total-execution-time ns, Pass Count: pass-count , Average: average-execution-time ns, Max: maximum-execution-time ns, Min: minimum-execution-time ns

[Example of use]

>>>debugger.Timer.Get()
1 Total: 2000 ns, Pass Count: 4 , Average: 500 ns, Max: 800 ns, Min: 300 ns
>>>