This function enables performance measurement. [RH850][E1/E2/E20/Full-spec emulator/IE850A]
If performance measurement was enabled successfully: True
If there was an error when enabling performance measurement: False
This function enables performance measurement of a performance measurement event number specified by performanceNumber. |
If performanceNumber is not specified, then performance measurement of all performance measurement event numbers will be enabled. |