|
debugger.PseudoError.Clear
|
This function clears the error status of all pseudo-errors. [RH850][E1/E2/E20/Full-spec emulator]
[Specification format]
debugger.PseudoError.Clear()
|
[Argument(s)]
None
[Return value]
If the error status of all pseudo-errors was cleared successfully: True
If there was an error when clearing the error status of all pseudo-errors: False
[Detailed description]
- | This function clears the error status of all pseudo-errors. |
[Example of use]
>>>debugger.PseudoError.Clear()
True
>>>
|