debugger.Jump.File

debugger.Jump.Address


This function displays each panel.

[Specification format]

debugger.Jump.File(fileName, lineNumber = 1)
debugger.Jump.Address(jumpType, adddress = 0)

[Argument(s)]

Argument

Description

fileName

Specify the name of the file to display.

lineNumber

Specify the line to display (default: 1).

jumpType

Specify the type of panel to display.

The panel types that can be specified are shown below.

Type

Description

JumpType.Source

Editor panel

JumpType.Assemble

Disassemble panel

JumpType.Memory

Memory panel

address

Specify the address to display (default: 0).

[Return value]

None

[Detailed description]

-

debugger.Jump.File displays the file specified by fileName in the Editor panel.
If lineNumber is specified, then the line specified by lineNumber in the file specified by fileName is displayed.

-

debugger.Jump.Address displays the panel specified by jumpType.
If address is specified, then the area corresponding to the specified address is displayed.

[Example of use]

>>>debugger.Jump.File("C:/test/testJump.c")
>>>debugger.Jump.File("C:/test/testJump.h", 25)
>>>debugger.Jump.Address(JumpType.Memory, 0x2000)
>>>