debugger.IsConnected


This function checks the connection status of the debug tool.

[Specification format]

debugger.IsConnected()

[Argument(s)]

None

[Return value]

If the debug tool is connected: True

If the debug tool is not connected: False

[Detailed description]

-

This function checks the connection status of the debug tool.

[Example of use]

>>>if debugger.IsConnected() == True :
...  print "OK"
...
True
OK
>>>