This function resets and then run the program.
[Specification format]
debugger.Run(runOption = RunOption.Normal)
|
[Argument(s)]
|
|
runOption
|
Specify an option.
The options that can be specified are shown below.
|
|
|
RunOption.WaitBreak
|
Wait until the program stops.
|
RunOption.Normal
|
Breakpoints enabled; do not wait until the program stops (default).
|
[Return value]
None
[Detailed description]
- | This function resets and then run the program.
If "RunOption.WaitBreak" is specified in runOption, then it will wait until the program stops. |
[Example of use]
>>>debugger.Run()
>>>debugger.Run(RunOption.WaitBreak)
|